Feedback_Calibration_Speed
Feedback_Calibration_Speed
| Address: | 10278 (2826H) |
| Type: | UINT16 |
| Access: | Read/Write |
| Unit: | 0.01 rpm |
| Range: | 0 to 10000 |
| Default Value: | 500 (5 rpm) |
| Store Supported: | Yes |
| Description: | This value is used for Feedback feature and define motor speed during the calibration procedure. The value must be set at low speed. Generally 5 rpm is a good choice. |
| Notes: | See Closed Loop Modality for details. |